Skip to Contents

Seismic Isolation

Seismic Isolation

THK Seismic Isolation Systems protect your property

A company's business continuity is often called into question. Many believe that business continuity requires an enormous amount of effort, but there are some things that can be done without major difficulty, such as installing seismic isolators that protect the valuable property of a company from earthquakes.

THK Isolation Module - Model TGS

 

THK Isolation Module - Model TGS

Model TGS isolation modules enable flexible layouts and are suitable for the partial isolation of heavy loads and seismic floor isolation.
(Maximum load: 3000kg per m2)

Applications: seismic floor isolation, semiconductor manufacturing equipment and large servers

Details


THK Isolation Table - Model TSD

 

THK Isolation Table - Model TSD

Model TSD isolation tables are seismic isolators that function by simply installing them on the floor. They have been adopted for a wide range of applications, including servers, precision instruments, and works of art.
(Load: 30 to 1200kg)

Details


THK Seismic Isolation Systems support buildings

We have combined multiple technologies to produce reliable support systems.

THK’s seismic isolation systems incorporate our core products, including LM Guides. These systems have been developed as applications of our products and reflect THK reliability, experience, creativity, and technological expertise.

Details(1,740KB PDF)

Linear guide CLB

 

Linear guide CLB

The linear guide CLB is a seismic isolation system that accommodatesa heavy sustained load with extremely low frictional force, since the balls in the LM guide rotate on raceways cut into the LM rail while circulating through the block. Since the LM block is equipped with an LM rail and balls, the bearings can also accept a pulling load.Contact THK for detail 


Viscous damping system RDT

 

Viscous damping system RDT

This system absorbs earthquake force transmitted to the building with the resistance offered by a viscous substance. The viscous damping system RDT has a structure in which linear motion is converted via a ball screw nut into rotary motion. A shearing force is applied to the viscous substance between the inner tube, which connects to the nut, and a fixed outer tube. Contact THK for detail 


Recovery system

 

Recovery system

When an earthquake occurs, houses with isolated bases can freely move away from their foundations in any horizontal direction. Therefore, they need to return to their original positions when the earthquake ends. For that purpose they are equipped with this recovery system, which incorporates laminated rubber and other materials.Contact THK for detail 


Contact Form